• Wood Yard
  • Fiber Line
  • Drying
  • Boiler
  • Paper Machine
  • Power Supply
  • Coatings
  • Services
  • Energy Efficiency
  1. Home
  2. Pulp & Paper - Fiber Line

Fiber Line

WEG supplies a complete solution to drive the shredder, one of the most important processes in the production of Pulp & Paper. The drive must be prepared for high inertias and high resistant torques to operate the shredder effectively.

A pony-motor can reduce the impact of drawing power direct from the grid to start the shredder which requires a starting current much higher than the rated current.

Our solution for the power supply of the refiner provides efficiency with the best cost effectiveness. Our CFW11 drive can be configured with two outputs using the same frequency drive for the Pony-Motor and the motor of the screw feeder. In this application, the motor and drive set is able to operate with constant torque throughout the speed range, in addition to withstanding momentary over speed when required.

Get to know our solutions

Three-phase Induction Motors - Master Line

Saiba mais sobre as novidades da WEG em Papel & Celulose

Supply for the Puma II project strengthens partnership between WEG, Valmet, and Klabin

Supply for the Puma II project strengthens partnership between WEG, Valmet, and Klabin

Investments in large-scale projects drive the growth of the pulp and paper segment in Brazil

WEG Drives the Sucuriú Project, Arauco's First Bleached Pulp Mill in Brazil

WEG Drives the Sucuriú Project, Arauco's First Bleached Pulp Mill in Brazil

WEG's technological solutions enhance efficiency, reliability, and sustainability in the pulp sector

WEG applies hybrid paper technology to transformers through R&D project

WEG applies hybrid paper technology to transformers through R&D project

Hybrid paper technology should extend the life of transformers

Growing interest in South Africa for steam turbine self-generation

Growing interest in South Africa for steam turbine self-generation

A 45 MW extraction backpressure steam turbine from WEG will be adding to Sappi Saiccor’s energy generating capacity at its MgO3 plant. The power generated will be used for internal consumption

WEG Portugal fornece 28 motores para projeto de inovação e renovação da DS SMITH

WEG Portugal fornece 28 motores para projeto de inovação e renovação da DS SMITH

Os motores foram produzidos na fábrica da WEG em Portugal

Soluções WEG equipam máquinas de empresa fabricante de tubos e tubetes de papelão

Soluções WEG equipam máquinas de empresa fabricante de tubos e tubetes de papelão

Por meio de um sistema personalizado o cliente já obteve um aumento de mais de 6% de eficiência em poucos meses

WEG fornece pacote de soluções para expansão de fábrica da Bracell no Brasil

WEG fornece pacote de soluções para expansão de fábrica da Bracell no Brasil

Fornecimento contemplou todos os motores, painéis elétricos, transformadores e inversores, totalizando mais de 6.300 itens entregues

WEG fornece pacote elétrico para nova fábrica da Suzano

WEG fornece pacote elétrico para nova fábrica da Suzano

Escopo envolve mais de 3 mil itens, entre eles: transformadores de distribuição, motores de alto rendimento, painéis elétricos e drives

WEG fornece pacote elétrico de R$140 milhões para expansão da Klabin no Paraná

WEG fornece pacote elétrico de R$140 milhões para expansão da Klabin no Paraná

Projeto Puma II faz parte de novo ciclo de investimentos da companhia e colocará no mercado 910 mil toneladas anuais de papéis

WEG conclui o mais completo fornecimento de soluções à WestRock

WEG conclui o mais completo fornecimento de soluções à WestRock

Turbogerador, eletrocentros, CCM´s, inversores de frequência, motores e transformadores tipo seco são os equipamentos fornecidos pela WEG.

WEG fornece motor de ímãs permanentes para Klabin

WEG fornece motor de ímãs permanentes para Klabin

W22 Magnet traz mais produtividade para a produção de papel e celulose

Cia Canoinhas reforça produção com equipamentos WEG

Cia Canoinhas reforça produção com equipamentos WEG

Maquinário de papel tissue recebeu motores elétricos W22 IR3 Premium e W50

Implementando atualizações para reduzir custos de manutenção e aumentar capacidade de produção

Implementando atualizações para reduzir custos de manutenção e aumentar capacidade de produção

Autor: Keith Kloiber, Gerente para a Indústria Papeleira, WEG EUA

Cia Canoinhas e WEG juntas no Programa de Eficiência Energética ANEEL/Celesc

Cia Canoinhas e WEG juntas no Programa de Eficiência Energética ANEEL/Celesc

Indústria economiza energia com motores de alto rendimento.

Over 2 thousand WEG products at Eldorado wood pulp plant

WEG offers products and services to the business unit which will be the largest factory in the world of the sector in a single line, empl...

Gostou da Solução e quer saber como adquirir? Escolha uma das opções abaixo e encontre o produto que você deseja:

Entre em contato com a gente e tire suas dúvidas.

Fale Conosco
WEG SINGAPORE PTE LTD
  • 67B Joo Koon Circle - 629082 / Cingapura
  • Phone: +65 6862 2220 / +65 9783 1399
  • Email: info-sg@weg.net
    ngjc@weg.net
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
  • Redutores e Motorredutores
  • Geração, Transmissão e Distribuição
  • Drives
  • Controls
  • Automação Industrial
  • Painéis Elétricos
  • Critical Power