• Collection and Irrigation
  • Automation
  • Power Supply
  • Coatings
  • Animal Comfort
  • Services
  1. Home
  2. Farming & Agriculture - Collection and Irrigation

Collection and Irrigation – Automation and use of alternators in the water collection system.

Essential for production in the farming industry, water usage must be optimized so as to improve the product quality and production between harvests, intensify the use of the land, and reduce the risks of investment in agricultural activity.

Seeking to maximize the efficiency of the processes and obtain the best economical return, WEG offers alternators to be coupled to the diesel generator set that supplies the collection pumps and the traction motors, as well as fertilization pumps and all electrical systems. These alternators, when coupled to diesel or gas engines (stationary), are responsible for providing the electric energy to supply all the power for the water collection system and also the pivot irrigation. WEG alternators are built following national and international standards, complying with the main application criteria and requirements.

For the irrigation system, the most recommended solution is to use soft-starters or variable speed drives. Using a WEG solution, it is possible to obtain high productivity rates and energy efficiency, bringing even more results for the farming industry.

Get to know our solutions

Soft-Starter SSW05
Soft-Starter SSW06
Soft-Starter SSW08
ASW06 Series
ASW07 series
SSW7000-Medium Voltage Soft-Starter

See more cases

See more cases

Case Cocari Grain Storage Case

Saiba mais sobre as novidades da WEG para o Agronegócio

WEG-CESTARI provides a complete solution to enhance energy efficiency at Yara Brasil Fertilizers

WEG-CESTARI provides a complete solution to enhance energy efficiency at Yara Brasil Fertilizers

WCG20 gearmotor line offers greater performance to the fertilizer industry

WEG equipment doubles thermoelectric power plant capacity in a food production company

WEG equipment doubles thermoelectric power plant capacity in a food production company

Bem Brasil is the largest potato producer in Brazil and has invested in the generation of its own power supply.

Why use WEG motors in agribusiness?

Why use WEG motors in agribusiness?

The increased need for new technologies in agribusiness, connecting people industry wide and the use of highly reliable equipment, makes all the difference in the productivity of farms.

TGM receives LIDE Agribusiness Award 2019

TGM receives LIDE Agribusiness Award 2019

The company was the winner of the LIDE AGRIBUSINESS 2019 Award within the “Agribusiness Technology”

WEG fornece motores à prova de explosão para uma das maiores plantas de amônia do mundo

WEG fornece motores à prova de explosão para uma das maiores plantas de amônia do mundo

Projetados e fabricados pela fábrica da WEG em Maia, Portugal, esses motores à prova de explosão irão acionar bombas d’água para alimentação das caldeiras e bombas de processo.

FS Bioenergia é pioneira na produção de etanol de milho no Brasil

FS Bioenergia é pioneira na produção de etanol de milho no Brasil

Usina conta com soluções WEG de alta eficiência

Zest WEG Group helps farmers to reduce their electricity cost

Zest WEG Group helps farmers to reduce their electricity cost

An effective strategy employed by some of South Africa's most successful farms is to replace the older, less efficient motors whenever they fail

Solução WEG com motores Cooling Tower Direct Drive System reduz custos em parque fabril da maior empresa de suco de laranja do mundo

Solução WEG com motores Cooling Tower Direct Drive System reduz custos em parque fabril da maior empresa de suco de laranja do mundo

Sistema modula a velocidade de acordo a demanda da aplicação, promovendo economia de energia e redução no consumo de água.

WEG Improves the Environmental Impact of the La Corona Sugar Mill in Argentina

WEG Manufacturing in San Francisco, Córdoba, recently installed the largest low voltage variable frequency drive (2280A) controlling a WE...

Sistema innovador para ventilación en silos reduce el consumo de energía hasta en un 80%

Este valor es superior a las medias anteriores de la solución WEG

Solución WEG reduce costos en la producción de arroz

Proyecto presentado por WEG ahorra un 70% en el consumo de energía eléctrica y disminuye desgastes de equipos.

Cambio de motores aumenta eficiencia en fábrica de BRF

La línea Wwash fue desarrollada para cumplir exigencias de las buenas prácticas sanitarias, al mismo tiempo que combina reducción de cost...

Eficiencia energética en Cargill

WEG suministra soluciones que garantizan productividad y ahorro de energía para la producción de alimentos desde las primeras etapas de l...

Gostou da Solução e quer saber como adquirir? Escolha uma das opções abaixo e encontre o produto que você deseja:

Entre em contato com a gente e tire suas dúvidas.

Fale Conosco
WEG GROUP AFRICA (PTY) LTD
  • 6 Laneshaw Street, Longlake Extention 4, Johannesburg, Gauteng, 1619 - Private Bag X10011 - Gauteng / África do Sul
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
  • Painéis
  • Tintas e Vernizes
  • Partes e Peças
Soluções
  • Oil & Gas
  • Naval
  • Siderurgia
  • Água
  • Eficiência Energética
  • Energia